This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61177A: Does using with PWM mode only is possible?

Part Number: TPS61177A

1. Can we use this device with PWM control only? as my board do not have interface available for I2C

2. will it be suitable for 9 LED strings with 3 LED's in serial (max IF 20mA, VF 3.2V for each LED), so combining all CS1 to CS6?

3. can we control the total backlit current to 180mA typically in above scenario?