This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Power-on initialization issue

Part Number: BQ76952

Hi team,

The customer has designed a BMS board and sometimes the initialization is successful and sometimes unsuccessful after a power-on reset. If the initialization is successful, an alert signal is generated and the BQ76952 register is set up for normal read and write. If unsuccessful, no ACK returned after BQ76952 address 0x10 was sent through the MCU's single-step trace debug. The reset signal is generated 100 ms high by the MCU GPIO and is connected to the RST_SHUT pin of the BQ76952.

The customer would like to know what to do with the BQ76952 after power-on initialization or reset. Could you help resolve this case? Thanks.

Best Regards,

Cherry