This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24195L: Setting up 5V output from SW pin

Part Number: BQ24195L

Hi there,

Just a quick question. I have the BQ24195L chip setup such that the SW pin is connected to a Power switch that requires 5V.

Based off the BQ24195L data sheet, the SW pin offers between -2 and 20V output.

My question:  Is there a specific register setup that allows for 5v output from the SW pin or is there a specific setup required to output 5v from the SW pin.

Thank you

Any help would be greatly appreciated