This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC5870-Q1: Vref drive capability?

Part Number: UCC5870-Q1

Hi,

I am wondering if the pin Vref can be used as a voltage source to power a resistor-NTC circuit, which requires less than 1mA? What is the drive capability of the Vref? Thanks.

Best Regards,

Shangjian

  • Hi Shangjian,

    Vref can take loads up to 5mA. Additionally I would recommend using one of the AIx ADC pins for NTC temperature sensing. Three of these pins (AI1, AI3, and AI5) have an internal current source that can be enabled to bias such NTC temperature sensing circuits. This current source is configurable through SPI and can source 0.1mA, 0.3mA, 0.6mA or 1mA.

    You can read more about our integrated ADC starting in section 7.3.3 of the UCC5870-Q1 datasheet.

    Best regards,

    Andy Robles

  • HI Andy,

    Thank you for the answer and the suggestion.  I assume you are referring to NTC diode. While as I am using a NTC thermal resistor, I simply configure AI pins as voltage sensing mode.  Is this application of Vref and AI pins suggested?

    Best Regards,

    Shangjian 

  • Thank you for the answer and the suggestion.  I assume you are referring to NTC diode. While as I am using a NTC thermal resistor, I simply configure AI pins as voltage sensing mode.  Is this application of Vref and AI pins suggested?

    Shangjian, 

    Even for NTC resistor, you would still use the internal current source to bias it. 

    The AIx pins are always in voltage sensing mode because they are ADC inputs. The configurable part is the current level that sources from the pin in order to get a voltage acorss the NTC resistor that the internal ADC can then read. 

    Configuration is like Andy stated in the last post. 

    Best

    DImitri