Hello team,
We are going to use UCC 28911 in our design and prepared proto board on UCC28911EVM-718 board by some changes
We have some queries regarding the same please address
Q1: Is limit for Drain Over current protection [Id(ocp)] will get change w.r.t. Ripk resistor used ?
As per datasheet, If Ipk pin shorted to ground then Id(ocp) is 980mA (typ.)
But, If we use Ripk (>900 Ω) then is the Id(ocp) will remain same as 980mA or will get changed ?
Like, if I use Ripk = 1200 Ω then will Id(ocp) remains same as 980mA or it will get changed according to below formula
Id(ocp) = VCSTE_OCP / Ripk
In this case new modified limit of Id(ocp) will be = 885/1200 = 737mA
Is it correct ?
Please confirm…
Q2: What is the significance of parameter Vcste (max) if I use Ripk = 1200 Ω (page 10 of datasheet) ?
Q3: Apart from above, we are facing start-up issue as described below
Note: Design specification and circuit diagram attached below
Design specification and circuit diagram.docx
Waveform details
Ch1: Drain voltage (Yellow) (100V/ division)
Ch2: Drain current (Green) (200mV/ division) (1mV=1mA)
Ch3: Voltage on VS pin (Blue) (5V/ division)
Ch4: VDD of UCC28911 (Pink) (5V/ division)
@ 36Vac, no load at Vout (with Pre-load 1K)

Zoom view

Why voltage on VS pin is continue increasing ?
It starts from 2V(at start of switching) and increasing till 5.1V and then stops
Please suggest some suitable actions to resolve the issue
Regards,
Sumersingh