This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: Terminate Charge TC vs Full Charge FC

Part Number: BQ40Z80

Hi,

What is the difference between Terminate Charge TC vs Full Charge FC?

Thanks,

Kim

  • Hello Kim,

    They are both similar functions, FC has more flexibility to show with the LED functionality to a user that the full charge has been reached. TC has similar thresholds to set and can be used by the MCU to indicate when the charge should stop, it can also disable the CHGFET when set if FET Options[CHGFET] = 1. A lot of the time these flags can be set together, that's how they are at default config when VCT is set. 

    All the information is in the TRM, section 5.7 Charge and Discharge Termination Flags

    Sincerely,

    Wyatt Keller