Other Parts Discussed in Thread: TPS61031, TPS63021, TPS61091, TPS63030, LMR62014
Hi,
We see that the TPS61130RSAR is in stock.
Is this IC recommended for our application described below?
- 2x alkaline C cell batteries in series (1.8 - 3.3V input)
- WiFi module (ESP32)
- Board operating voltage: 3.3V
- Average power consumption: 200mA
- Peak power consumption (during WiFi transmit)): 500 mA
The device will be in deep sleep about 95% of the time.
To maximize the utilization of the C-batteries we need a 2000uF capacitor on the output of the buck-boost to avoid early brownout.
Thanks.