Hi team,
Issue: When designing a 20S BMS with the BQ7693003, neither BQ chip can enable the internal ADC. The status register value is 0, the ADC_EN value in control register 1 and the CC_EN value in control register 2 are 0, and the voltage cannot be read.
the customer would like to know if it is because the chip is collapsed and cannot be used anymore.
Could you help resolve this case? Thanks.
Best Regards,
Cherry