Other Parts Discussed in Thread: BQ76952
Hi,
We encountered two problems when using BQ76952EVM.
a) bqsbb after the upper computer sends the shutdown() command_ When CMD is set, FET can be closed normally, but bq76952 does not enter shutdown and can continue communication. Reg1 can output 3.3V. It is found that the voltage of TS2 is 0.1V and the resistance of TS2 to GNG is 7.8M
b)After sending deepsleep() command, pressing reset button for a short time cannot wake up DEEPSLEEP mode. After briefly pressing the key, the upper computer still displays DEEPSLEEP set and sends exit_ deepsleep() can exit DEEPSLEEP mode. No current enters SLEEP mode, SLEEP is set, and SLEEP is cleared by short pressing the key.
We look forward to your reply! Thanks!