Hello,
I am using BQ24170 charger IC and associated circuit for charging a lithium Ion 3S2P battery pack with a charging current of 1.5A. The battery and charging circuit is part of a medical device. The design works perfectly so far. For 60601-1 medical device safety , we need to simulate a single fault condition i.e we need to short the current sense resistor connected across the SRP and SRN pins of the BQ24170. As per Design it is 10mohm on the PCB, but our plan is to short it( which means it will be close to 0ohm). We want to see what is behavior of the circuit in that scenario. We have 2A Fuse both at AC adaptor and battery power lines respectively, so that in case the current exceeds this limit, the fuse will open up.
I would like to know what is the possible/expected behavior with this sense resistor value manipulation. Will there be any other protection from BQ24170 which can trigger?
As this is likely to be a destructive test, I want to know if the behavior can be predicted.
Attached is the schematic for reference. Just note Fuse F1 and F2 both are 2A( although one of them in the attached file is shown as 3A rated)
Thanks,
Siddharth