Part Number: TLV758P
Other Parts Discussed in Thread: LP5912, TPS745,
Hi Team,
There is a good new that Customer is searching TI solution
Do we have a product that can compete with "MAX8902BATA+" ?
Does TLV75801PDBVR is a good solution?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV758P
Other Parts Discussed in Thread: LP5912, TPS745,
Hi Team,
There is a good new that Customer is searching TI solution
Do we have a product that can compete with "MAX8902BATA+" ?
Does TLV75801PDBVR is a good solution?

Hi Kygo,
TLV758P is ok if they do not need PG, but I think TPS745 or LP5912 are better options assuming they need the PG function.

Text version
| MAX8902B | TPS745 | LP5912 | |
| AEC Q100 | YES | NO | NO |
| Output Options | Adjustable Output | Adjustable Output | Fixed Output |
| Iout (Max) (A) | 0.5 | 0.5 | 0.5 |
| Vin (Max) (V) | 5.5 | 6 | 6.5 |
| Vin (Min) (V) | 1.7 | 1.5 | 1.6 |
| Vout (Max) (V) | 5.3 | 5.5 | 3.3 |
| Vout (Min) (V) | 0.6 | 0.55 | 0.9 |
| Fixed Output Options (V) | ADJ | - | 0.9, 1, 1.1, 1.2, 1.5, 1.8, 2.5, 2.8, 3, 3.3, 5 |
| Enable | YES | YES | YES |
| Power Good | YES | YES | YES |
| Output Capacitor Type | Ceramic | Ceramic | Ceramic |
| PSRR @ 100KHz (dB) | 55 | 45 | 40 |
| Noise (uVrms) | 16 | 53 | 12 |
| Accuracy (%) | 1.5 | 1 | 3 |
| Vdo (Typ) (mV) | 150 | 95 | 150 |
| Iq (Typ) (mA) | 0.08 | 0.025 | 0.03 |
| Thermal Resistance θJA (°C/W) | 83.9 | 80 | 71 |
| Min Package Area (mm2) | 4 | 4 | 4 |
| Package Type | WSON | WSON | WSON |