This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: CycleCount() does not increment after a full discharge

Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQSTUDIO

Hi, 

I am currently trying to discharge a battery from fully charged (12200mAh remaining capacity) to 0% (0mAh remaining capacity)

The problem i am having is that the cyclecount() does not increment after a full discharge, 

PS: i have the [CCT] = 0 and design capacity is set to 12120 mAh (6060 * 2)