Hello to TI support team ,
I have application of 8S9P --> Design Capacity 31050mAh , Max Current 80A .
As I read some TI tutorial before , there is problem with Capacity more than 29Ah and Current more than 32A .
according to TI paper There is solution with X10 bit ( 7 bit in Pack Configuration low byte) and scale ( 5 bit Pack Configuration high byte) , I use LOAD 0 ( mAh indication ) .
1. What is the proper solution for my design ( X10 bit , Scaling bit or another) ?
2. Can I prepare Golden Pack file without X10 and scaling and set it only at the end of process ?
B.R
Alex Burtakov