This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
I want to evaluate the thermal performance of TPS7A92. Here I have some questions about the thermal metric for TPS7A92
Thanks.
Hi Kelly,
Regards,
John
Hi John,
we leverage thermal shutdown temp 160C at steady state together with power loss at this time, and place a thermocouple at the top case of TPS7A92 for case temp, but the thermal resistor calculated is about 16C/W which is much higher than the datasheet Psi_JT(0.8C/W), is this reasonable and why?
thanks.
Hi Kelly,
No I would say that that is a bit too far off from how the part should be behaving.
This document details the testing conditions to get a true Psi_JT value. Assuming 160C as the shutdown temperature is the first place that I would say error may be arising from, the next place would be that you state steady state operation, in thermal shutdown the part should be switching on and off, if it is not, then it must be below it's thermal shutdown temperature which would increase the perceived thermal resistance. If the part is switching than the fluctuations in power dissipated and temperature seen would also cause instability in the accuracy of the reading, which is why JEDEC testing requires the actual Junction temperature to be measured in order to assure you receive an accurate psi or theta measurement. Both of these cases would cause the thermal resistance to be computed as much higher than it is actually performing
Regards,
John