Other Parts Discussed in Thread: UCC20520
Can a single PWM signal drive a dual input driver?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
It is sometimes necessary to drive a dual input driver (A driver with two individually controlled channels) with a single PWM input. This could be because of a limitation in the controller used, or PCB layout considerations. The easiest solution is to simply use a PWM input driver such as the UCC20520, but sometimes a different UVLO or package is required. The below external circuit can be used in these situations to create complementary inputs from a single PWM signal.
As shown in Figure 1, a simple transistor based inverter can be used to invert the signal for INB, while directly connecting the PWM signal to INA. This is effective because the deadtime can be controlled by the driver, making it less important to match the propagation delay of INA and INB.


If you have more questions about this, or related issues please click the button in the upper right to ask us a question.