Hi,
I check datasheet and the device support input voltage range is 4.5~18V.
My customer design is output voltage=1.8V, the input voltage=4.5V is ok for the design, right?
The other question is the device has max duty cycle spec?
For example, if output voltage design is 5V, what is the min input voltage requirement?