For example, I set OCD1 delay to 4 seconds and OCD1 Threshold to 4000 mA in my data memory
When i discharge my battery with a current of 5000 mA, i have the good delay (4 seconds) between OCD1 Alert Flag and OCD1 Status Flag. But i record the current and voltage with an external device and i have a delay between the start of discharge and OCD1 Alert Flag and a delay after OCD1 Status Flag and the end of discharge.
My opening mosfet is very fast (microsecond), so i don't have a delay between command signal and opening. I thinks that the first delay the BQ40Z80 reading too late the current and the second delay the BQ40Z80 activate too late the Mosfet.
I have about 1.5 seconds longer, so 5.5 seconds between the start of current and opening mosfet, it's normal ?