Part Number: LM76005
Other Parts Discussed in Thread: LM61495, LM61480, LM25149
Hi Team,
Does LM76005 support 5A input current?
Best Regards,
Gust
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gust,
I would suggest picking a higher current rated device is you want to operate at 5A input current.
The is not capable of 100% duty cycle so the input current will always be lower than the maximum rated 5A current limit of the device.
Perhaps the LM61480 or LM61495 might be more applicable for your design requirements.
Regards,
Jimmy
Hi Jimmy,
Thanks for your reply. I want to find a suitable DCDC that the input is 48V/5A and output is 24V/4A. Do you have any recommendation?
Regards,
Gust
Hi,
Can you help me understand your application more on why the input current must be 5A?
Normally the input current for a buck converter is lower than the output current.
Currently there is nothing in the converter portfolio to satisfy your application so I'd suggest look at controllers such as the LM25149 which was recently released.
Regards,
Jimmy