The thermal resistance of the WEBENCH simulation result is described as 26 °C/W(θja). However, the LMR14050 Spec Sheet has a description of 42.5°C/W(θja). I would like to know what kind of heat dissipation conditions each has. Regarding heat dissipation, there is a description that please refer to SPRA953 , but I can not understand the details, so please let me know. The thermal resistance of the TO-220 package only is 60°C/W, so the HSOIC-8 without a heat dissipation mechanism is above that value.
Simulation parameters
VinMin = 18.0V
VinMax = 20.0V
Vout = 9.0V
Iout = 4.5A
Device = LMR14050SDDAR