Other Parts Discussed in Thread: BQ25611D, BQ25611
Dear in-charge person.
We evaluate BQ25600D and our LIB samples.
<Our current situation>
When IC temperature status is typical, we can observe ordinaly charge termination.
But when IC temperature status is cool, we cannot observe charge termination.
Our charge termination current setting is 120mA.
As our analysis, when IC temperature status is cool, we detect error as charge safety timer expiration , becuse IC cannot stop charge at 120mA.
<Question>
1. When IC temperature status is cool, charge current setting got 0.2C.
Similary, do charge termination current get 0.2 times(24mA), or keep set current (120mA)?
2. We need to stop charging at 120mA. Is there present example and solutions about above trouble.
Thanks