Hi Expert,
I don't really understand what's the current limit for each channel. I don't see clear description about this. what does it mean by "The maximum output current from....phase configuration"? The total current is less than 10A and for the same time each channel output current is less than 4A or 3A depending on input voltage if I use 4 1-phase?
As for LP87524b/j/p-q1, things are a little different as below. Are the output current limit are fixed as below? Only depending on input voltage sometimes?
BR,
Elec Cheng