Hello TI Team,
I am using the Transient PSpice model provided in TI website for LMR33630A. I have an input of 12VDC and I want output of 5VDC at output.
I have designed the circuit as per requirement but when I simulate it in LTSpice I get a Transient of 12V at output and post that the 0V is arriving. (Attached is the simulated result).
I have connected the VCC output(5V) internally generated to the PG Pin through a 100K Resistor and a bypass capacitor of 1uF but at the PG I am getting 30mV. When a 2V DC source is directly connected to PG pin I am getting a simulation error.
Can anyone guide me here on why is this happening? Am I using the right Spice Model?