This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23753A: TPS23753A specification of the next transformer

Part Number: TPS23753A
Other Parts Discussed in Thread: TPS23734EVM-094

hi:

The transformer corresponding to TPS23753A is used for POE +, with an output of about 25W and an output voltage of 12V.

Please help provide the specification of the next transformer

  • Hello, 

    Which TPS23753A design are you referring to? Is this one of the EVM's or a TI Reference Design? 

    Additionally, the TPS23753A is only rated for 13W, so it cannot be used in a 25W design. A 12V/25W design is the TPS23734EVM-094. 

    If this post answers your question, please indicate so by marking this thread as resolved. Thank you.

     

    Regards, 

     

    Michael P.

    Applications Engineer

    Texas Instruments