Relation between Input current and the output current of the inverter.

The input to the inverter is 12V Battery and motor is for example is continuous is 2KW and peak is 4KW. I have few questions here
a. If the operating voltage of the inverter is for example from 9V to 15V, the Peak input current of the inverter is 4KW / 9V = 444 Amps and the continuous input current of the inverter is 2KW/20V = 222 Amps. Are my calculations correct? Please help.
b. I don't know how to calculate the Irms and the Vrms values at the output of the inverter Irms_peak, Vrms_peak, Irms_continuous, Vrms_continuous. Any support i can try and derive.