Hello,
We are working on AFE BQ7694001 with companion IC 14Sseries. Please find the attachment for the schematic.
we are facing a suitation where at voltage reading at the pins with IC and without IC are as follows mentioned in the table.
VC0 |
VC1 |
VC2 |
VC3 |
VC4 |
VC5 |
VC5B |
VC6 |
VC7 |
VC8 |
VC9 |
VC10 |
VC10B |
VC11 |
VC12 |
VC13 |
VC14 |
VC15 |
|
With IC |
0 |
3.8 |
7.6 |
11.5 |
15.3 |
19.1 |
19.1 |
22.9 |
27 |
31 |
35 |
39 |
39 |
43 |
47.1 |
51.1 |
51.1 |
55.2 |
Without IC voltage at pads |
0 |
3.8 |
7.67 |
11.5 |
15.3 |
19.25 |
28.26 |
28.28 |
28.3 |
30.8 |
30.6 |
30.02 |
38.1 |
42.1 |
47 |
51.1 |
51.1 |
55.1 |
Afer the IC is placed the Voltage measured by multimeter wrt ground from VC5B to VC10B is abnormal.
Also after When the IC is being soldered R51,R45 and R52 is starting to bleed.
Kindly review the schematic and let us know what are we missing, else what might be the cause os abnormal voltage readings.
Note: If IC is removed then the Voltages at the Pads are showing normal readings
Thanks in Advance