This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM26003: Check the VBIAS Pin of LM26003 for Inverting Applications

Part Number: LM26003


Hello

My customer designed inverting circuit using LM26003.

VIIN : +15V

VOUT : -12V

However, the maximum VBIAS voltage is 10V. Is it available to configure the circuit as shown below? 

Best regards.