Hi TI Team,
Let us say, We are using the part BQ25601RTWR in our current design and we are facing an issue with the input source.
Without battery, only with the input source (WIR_VCC_SYS =4.2V), there is no output voltage but at the boot pin can see 3.6V and there is no voltage at the switching node.
Without/with input source and with battery circuit working fine, getting proper voltage at VCC_SYS.
Any suggestions why is this happening?