Hi All
The thread was locked, so I'll post a new one.
I have a question about LMR12015.
I would like to know the minimum load current value under the following conditions.
- VIN=15V
- VOUT=12V
- L=3.3uH
I referred to "7.3.3 High Output Voltage Considerations" in the data sheet, but it didn't meet the conditions.
Is there any reference material such as the graph of "7.3.3 High Output Voltage Considerations"?
Or, please tell me the load resistance that can be switched without fail.
Best Regards,
Ishiwata