This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps65070 touch pressure with battery

Other Parts Discussed in Thread: OMAP-L138, TPS65070, TPS65070EVM-430, AM1808

Background: omap-l138 SOM running the linux psp

I am having an issue with the tps65070 when I try to read the pressure of the touchscreen and I am running off a battery.  Every reading comes back as 0x3ff.  This is not the case if I am powered by either AC or USB.  Scope traces of the touchscreen lines look fine when touch is applied, and the values given back as x/y measurements look valid -- it is just the pressure measurement that is wrong (0x3ff regardless of touching the display or not).

Any ideas?