Other Parts Discussed in Thread: USB2ANY,
Our customer bought TPS65217EVM, they followed all the jumpers.They did pump 3V3 and 5V into the evaluation board and still no output. Can anyone guide us how should they set for the evaluation board?"
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tharini,
Thank You for using E2E! Could you please provide the information below so I can better understand the issue and provide feedback?
Thanks,
Brenda
Hi Brenda,
here the answers:
TPS65217CEVM
Supply 3.3V externally
Follow the one recommend in the evaluation board settings
Apply 3V3 on 3P3 and ground on connector J8
Try applying 5V on BAT/AC/USB with respect to GND
There is no voltages at any of the outputs.
Kind regards,
Marion
Hi Marion,
Thanks for providing the information in the previous message! The scope capture that I requested before is important to evaluate the signals on the power path that supplies the PMIC rails. The output voltage from the converter can be excluded as there is no output voltage but AC, USB, SYS and PWR_EN are critical because they are input signals to the PMIC. If the customer could also provide a picture of their setup, that would be great.
Since the USB2ANY is not used, I suspect the external 3.3V is probably not being applied to the right pin on the J8 connector. Can they try the suggestions below and let me know if they see any difference?
Thanks,
Brenda