This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25040: Using charger without host MCU

Part Number: BQ25040
Other Parts Discussed in Thread: , BQ25170, BQ24040

I am using the bq25040 at a standalone battery charger for a single LiPo battery. There is no MCU on this board and I would like to program the fast charge current to ~500mA. It seems that this part is designed to be used with an MCU to set the current via the EN/SET pin, but in my case this isn't possible.

Can I set the charge current to be 500mA without needing to pulse this pin? It seems that the default current is USB500 (~400mA) without pulsing the pin, so I guess this is the only option, or am I missing something?