My team and I are building an avionics system for a student-led rocketry project in which we will be using a 2S2P configuration (we had recently switched from 4S1P) for our batteries. Is it right to take our measurements for each 'battery cell' at the following points in the cell configuration?

Readings will be taken from the 'most positive node' at vBat, then through a parallel connection at Bat_term_1, then a connection to the most negative node at GND. These will be respectively fed into VC2, VC3, and VC4 (unsure about this as well, perhaps VC5 should be used as the default 'most negative' node reading regardless of configuration)?
In addition, kelvin connections will be made as recommended by the manual.