Part Number: TPS2597
The data about the temperature raising of the device, and its safe range of output capacitor is missing during start-up. using the Excel tool (slvrbj2.zip file) shows that on most condition above 34degs the chip in not on 'successful startup'.
looking further, it seems that the Excel has bug. On Cell C7, TAB TSD. the formula there failing any start up above 34.01deg:
IF(AND(F6<34.01,E6<146.01),"YES",IF(AND(F6<36,E6<160),"MARGINAL",IF(OR(F6>=36,E6>=160),"NO","Unable to decide")))
My guess that this is bug, the number should be 134.01 (or something like that)