This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1HB08-Q1: output resistance

Part Number: TPS1HB08-Q1


Dear expert,

When TPS1HB08-Q1 EN is LOW, is there any resistance from VOUT to GND inside TPS1HB08-Q1?

Thanks

  • Hi Ryan,

    When EN is low, VOUT to GND resistance should be large enough to be treated as an open circuit. This is the working mechanism of the open-load detection as we use the 1Mohm resistor from VS to Vout to pull the output voltage to VS during open-load condition.

    Regards,

    Yichi