Hello all,
I am using the TPS7A1118 to provide1.8V with the following set up, to supply an ADC:
-Vin = 3.3V
-Vbias = 3.3V
-EN = 3.3V (all 3 pins are tied to 3.3V power plane)
-The NC pin is not connected, and GND pin tied to thermal pad to ground.
I can measure on Vout with multimeter 2.4V when supplying with 3.3V. with a range from 0 to 4V for Vin, Vout will vary from 0.12 to 2.58, and Vout will be 0 whenever Vin < 2.1V.
I checked for everything on pcb (shorts, some residual flux,...) nothing wrong... Is there something I am missing, with input pins range ?
I would be glad if you could enlighten me !