Part Number: UCC28782EVM-030
Other Parts Discussed in Thread: UCC27712
Hello
I have an issue when I change to use silicon (Si) power FETs on the primary side,
due to i would like to use silicon (Si) power FETs on the primary side,
I have reworked the SET pin connection (SET pin connect to Ref pin and make sure disconnect to AGND on EVM),
but it goes to DCM at 115Vac/20Vdc/3.25A, not BCM
could you help me to optimize to operating in BCM.