This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62141: DC/DC step-down power source

Part Number: TPS62141
Other Parts Discussed in Thread: TPS629210-Q1, TPS629210,

Hello,

We need any DC/DC convertor with input power supply (7.2V to 15V) and output voltage 3.3V or 3.8V and Iout(max) = 2A. And we need high efficiency power source and low power consumption (supply from solar panel). We would like to use TPS62141RGTR. I know that is this version have fixed 1.8V but the adjustable version in not available (TI, Digikey, Mouser, Arrow, Avnet). 

www.rocelec.com/.../TISTPS62141RGTR

Is it possible change the output voltage by external resistor?  

  

What is the value of the internal resistor R1, R2, R3? Could you write me the value of the Rext for the output voltage 3.3V or 3.3V? 

If is not this source suitable, could you write me better solution with other circuit that is available in Digikey, Avnet, Arrow or Mouser? 

Thanks and Best Regards. Tomas.