This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25890H: LOWER VSYS AND DOESN'T START CHARGING

Part Number: BQ25890H


Good evening,

I have a question about the BQ25890H single cell charger IC. After checking the evaluation board a few months ago, we built our first prototype boards per EVM schematics.

On the prototype board the VSYS is without battery 3.65V , which should be normally 4.2V and with battery connected, it follows the battery voltage which was for instance 3.85V. Connecting external power source @ 12.5V & 3.5Amax the BQ doesn't start charging. Power source consumption remains at 3mA and the LED is blinking @1Hz as if the battery was not present.

When load is present up to 2Amps that was tested, no abnormalities detected, even with/without battery and both sources connected.

The registers setup was carried over from the EVM which worked as it should.

Do you have any suggestion about what the problem could be?

Thanks and kind regards,

Georgios