We are looking at TPS23757, which is designed for 13W PoE. Can we use it in 18W output? What limits the application?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
You could use the dc/dc controller portion of the TPS23757 to control an 18W power supply (for an adapter powered dc/dc converter). For power applied over an ethernet cable (type 1 PD is limited to 13W at the RJ45 connector input), a compliant type 1 PD must limit it's input power to 13W.
For higher power applications (up to 25W), a type 2 compliant PD is required. You can use the TPS23754 or TPS23756 for this case.
Glad the E2E site is back up. It went down while I was completing this post last night, near midnight PDT.
There are many circuit factors in the design that are targeted at specific output power under certain conditions.