Hello,
We are trying to test a deeply discharged battery recovery using the BQ27742-G1 for a battery that has been discharged to a very low voltage. We measured the battery terminals at 2.7V which I believe should be above V_UVP.
If in low voltage charging mode the charge FET (CHG) is connected to the pack voltage (PACKP). Is this an internal short? If the gate of the CHG FET is not shorted to PACKP, it will follow 2xVPWR as shown in section 6.8?
From section 6.7, is VCHGATT configurable to lower than 2.7V? Our charger provides 2.0 fixed in pre-charge state and might not be enough for the FG to detect charger? Please let me know your comments on this as well .
We are applying 5V to charge the battery.
If we connect the discharged battery to an external power supply, I am able to start charging when I supply ~3.45V. Below this voltage, the battery does not charge. I am not sure what parameter this voltage corresponds to or if it’s configurable.
Thanks