Other Parts Discussed in Thread: TPS63900
Hi,
I'm trying to ramp the input voltage to this chip with enable ON or tied to the input with a 100 Ohm resistor. When I do that it gets stuck at 1.57V on the input and about 2-3V on the output, sinking any available current at the input till it current limits. Could you please advise on why this is happening and how to work around it?
I've also noticed that at any point if this part is starved with power on the input in boost mode operation, it also gets stuck in the same way as described above. My expectation in this scenario is that the part would pull the output voltage down and recover to normal output voltage when enough power is available on the input. Could you please advise why this is not the case and if there is a way around it?
This is a custom PCB. I should also mention that if I ramp the voltage while enable is OFF and then turn it ON, everything works as expected.