This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23751: Maximum value of Css

Part Number: TPS23751


Dear Specialists,

My customer is evaluating TPS23751 and has a question.

I would be grateful if you could advise.

---

Regarding CSS of Figure 36 of the datasheet P.37 8.2.2.14,

Could you please let us know the maximum value of  Css.

Is there any effect on other circuits by increasing the capacity of Css?

---

I appreciate your great help in advance.

Best regards,

Shinichi

  • Hello Shinichi,

    The maximum recommended value is 10uF. This capacitor is part of the secondary soft start circuit, which helps the output voltage not overshoot during startup. The larger the capacitor, the slower the turn on is. 

    If this post answers your question, please indicate so by marking this thread as resolved. Thank you.

     

    Regards, 

     

    Michael P.

    Applications Engineer

    Texas Instruments 

  • Hi Michael,

    Thank you for your reply.

    I understand the maximun recommended Css is 10uF.

    When the larger capacitance is used, the turn on is slower.

    I'll share this information with the customer.

    I appreciate your great help and cooperation.

    Best regards,

    Shinichi