This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: TPS1663

Part Number: TPS1663

Dear Madam/Sir,

We intend to use the TPS1663 as per clause 9.4 of IEC/UL61010-1.

UL file E169910 only lists TPS1663 up to a maximum current of I(OL) = 4.815A.

Please advise if TI intends to update the UL file with (up to) the I(OL) = 6.42A option, as per the TPS1663 datasheet.

Thank you!