Other Parts Discussed in Thread: UCC29002
..
Hi,
I am seeing UCC29950 is a very good PFC + LLC controller that can give > 90% AC to DC peak efficiency in some case even 94% and single IC operation. I am designing a power supply module for universal- AC input and 100W, 20V output. I have a paralleling requirement which means if needed user can parallel these 2 to 3 modules together to increase the overall power output.
Now I am afraid that the LLC converter may not be easy to parallel. By literature, in general for LLC paralleling , it seems it needs sophisticated DSP to do paralleling for LLC, I don't know if the small analog IC can work with another converter in parallel. Can we parallel the UCC29950 based design without any major trouble? like Forward or flyback topologies?