Hi,
In datasheet of this part, the capacitors and inductors indications is out of date, I want to check if this of I have selected is ok
My application: 250mA Máx load, 3.3V fixed, Vin 24V.
Inductor: 150uh 0.71A Würth Elektronik 744787151
Capacitor in: 68uF 80V 270mA Vishay MAL214699705E3
Capacitor out: 100uF 6.3V 595D107X96R3C2T
Diode: VS-10MQ060-M3/5AT
Thank you