Hello, I am using the PTH08T2xx series of devices in a Xilinx Virtex6 design and would like to drive the Smart Sync from the FPGA.
To do so the PTH08 must startup in free-run mode (300kHz) and then once the FPGA is loaded it would drive the Smart Sync pin at 240kHz.
Can I use a pull down resistor to GND on the Smart Sync pin and attach it also to the FPGA output? Then during Boot and Config of the FPGA the Smart Sync pin is held low and after that the 240kHz starts up. (See sample schematic below).
Also is there any disturbance on the Vout when moving from 300kHz to 240kHz switching?
Thanks, Al...