This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21222-Q1: Support 100% Duty cycle

Part Number: UCC21222-Q1
Other Parts Discussed in Thread: UCC21222

Hi team,

My customer would like to use UCC21222-Q1 in buck topology. I see in datasheet each channel can be controller independently.  May I know if UCC21222 supports 100% duty cycle?

Thanks,

Scarlett

  • Hi Scarlett,

    To determine whether this device can support 100% duty cycle will depend on additional details of the design:

    • Will both high side and low side need to support 100% duty cycle?
      • Could you give more details this 100% duty cycle operation?
    • Will both high side and low side have its own isolated bias supply or will they use a bootstrap circuit?

    Let us know if there's any questions.

    Best regards,

    Andy Robles

  • Hi Andy, 

    - Buck circuit input voltage is close to output, therefore I think only only high side needs 100% cycle,

    - Customer can use isolated bias supply. Bootstrap circuit cannot achieve 100% since need time to charge the cap, right?

    Thanks,

    Scarlett

  • Hi, Scarlet,

    That is correct. We would need to calculate it, but unless it goes high for hundreds Of milliseconds or more, the bootstrap should work. 

    are they having problems with an existing circuit, or just working on a new design?

    Best regards,

    Don

  • Hi Don,

    Thanks for your quick reply. It is a new design. Customer needs a buck circuit with Input voltage around 14V and output around 12V, since both input and output varies, for worst case customer is considering 100% duty which when input very close to output. Customer need dual channel iso driver since control on different GND. 

    Thanks,

    Scarlett

  • Hi Scarlett,

    The UCC21222 can support 100% duty cycle if using isolated bias supplies instead of a bootstrap. 

    Regards,

    Krystian