Hi,
Need design review of the below design:

Need to know if the FET selected is K, considering the PWM switching frequency is around 200 - 300 KHz. Also, is the inductor selected is good.
Input voltage typical is going to be 48V, output voltage expected is 24V. Here are the LED strips it needs to drive along with the calculator:
5047.TPS92660_Calculator_20220112.xlsx