This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61089: Can it be used as a tunable output with external analog signal injected to FB?

Part Number: TPS61089


Hi Expert

As the title, could TPS61089 be used as this way in theory? User case is 5V input, output 8V to 9V tunable. 

Thanks!

-Rocky