LMR23610 will work on PFM mode when light load.
What's the specific relationship/formula between work frequency and output current/input output voltage/inductance value?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LMR23610 will work on PFM mode when light load.
What's the specific relationship/formula between work frequency and output current/input output voltage/inductance value?
HI Huanghai:
see below description:
At even lighter current loads, PFM is activated to maintain high efficiency operation. When either the minimum HS switch ON time (tON_MIN ) or the minimum peak inductor current IPEAK_MIN (300 mA typ) is reached, the switching frequency decreases to maintain regulation. In PFM, switching frequency is decreased by the control loop when load current reduces to maintain output voltage regulation. Switching loss is further reduced in PFM operation due to less frequent switching actions. The external clock synchronizing will not be valid when LMR23610 enters into PFM mode.
so as the inductor average current is output current, the peak of inductor current is 300mA, with Vin, and VO, you will have Ton(inductor current raising time) and Toff((inductor current falling time) ) . 0.5*Ipeak*(Ton+Toff)/Tperiode=Io
frequency=Io/(0.5*Ipeak*(Ton+Toff))
Thanks